Skip to main content
January 14, 2023
Question

When will full support for vectors appear?

  • January 14, 2023
  • 0 replies
  • 481 views

I want to write simple c=a+b level code that will always give the same result, but use the maximum of possibilities.

Only 4 direct execution options are available for your architecture

typedef int8_t vi8_4 __attribute__ ((vector_size(4),aligned(4)));

typedef int16_t vi16_2 __attribute__ ((vector_size(4),aligned(4)));

typedef uint8_t vu8_4 __attribute__ ((vector_size(4),aligned(4)));

typedef uint16_t vu16_2 __attribute__ ((vector_size(4),aligned(4)));

And set at vector_size (4*n) through the built-in loop.

GCC recognizes vectors for A8 and above from the NEON library. It turns out very nice and compact.

And you get it https://godbolt.org/z/asbKj4rns

    This topic has been closed for replies.