What should be the HSE (bypass clock source) characteristics for STM32F7 to work fine?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-02-06 9:03 AM
Hello everyone,
I have an STM32F765VI MCU. When I work with internal clock it works fine. But when I switch to an external TCXO, It does not work properly. The TCXO output is a 26MHz sine wave with 1.5V peak to peak.
Does anyone know what may cause this problem?
What is the minimum amplitude of external clock which MCU can detect?
Thanks
Labels:
- Labels:
-
RCC
-
STM32F7 Series
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2021-02-06 1:01 PM
Should be in the Data Sheet - "High-speed external user clock characteristics"
VIL is 0 to 1 V
VIH is 2.3 to 3.3 V
Expect you'd need to buffer or center the sine for it to work. Could try the non-bypass mode
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..