cancel
Showing results for 
Search instead for 
Did you mean: 

What SDIO interface chip (with a 3.3V host side) are people using these days? The IP4856CX25 (used on the H7 Eval board) is NRND.

chriscole
Associate III

What SDIO interface chip (with a 3.3V host side) are people using these days? The IP4856CX25 (used on the H7 Eval board) is NRND, and I can't seem to find an SDIO interface chip that supports a 3.3V host side. What part should I use for a 3.3V H7 design?

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
tyassin
Associate III

Hi
Just picking up on this thread.
Interested if there was any results between SDR50 vs SDR104?