Question
What is the default value for PLLON ? If it is 0, should I put a while(PLLRDY =1)?
I have an application running on HSE as system clock..and I set the multiplexer to select HSE, totally not using PLL
btw, should I put any configuration to my PLL?
such as PLLON =0, and while(PLLRDY==1) , to “properly configure�? the unused PLL?
Or should I just leave it as what it is by default?
best regards,
mike