cancel
Showing results for 
Search instead for 
Did you mean: 

What is SAI "Error between selected"? (CubeMX bug?)

TDJ
Lead

Today I spent some time to fine-tune SAI clock to get standard 22.05kHz sample output rate.
However, I do not understand why CubeMX states that "Error between selected" is 0.22%.

What is "Error between selected"? Why this error is zero when selected frequency actually differs from the desired value by 0.05kHz? Am I missing something?

SAI3.png

SAI2.png

SAI4.png

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

@Piranha I totally agree, what I did was probably an overkill, but it was intentional. However, there are studies which indicate that some humans can tell 0.03% absolute frequency difference. Ofc, this is very rare, even among musicians. This topic is interesting in itself.