Skip to main content
mete
Senior
Sep 4, 2024 11:20 AM UTC
Question

what does TZEN really do ?

 

I know TZEN is used to enable TrustZone. At first, this made sense, but now I think about the MCU implementing the Security/TrustZone, and it sounds strange that TrustZone can be disabled. So my question is, what does it really do ? Does it really somehow disable (power down?, clock gated?) the TrustZone related things (SAU, GTZC etc.) ? so there is really a signal somewhere inside the die that enables/disables this. Or, is the TrustZone in the core always enabled and TZEN just reconfigures things so everything runs like a secure binary or maybe nothing generates a security fault ?

This topic has been closed for replies.

8 replies

Lead II
Sep 5, 2024 12:26 AM UTC

TrustZone is not related to power or clocks (not directly directly).
It just means: only code running on TrustZone domain (e.g. inside a TrustZone enabled memory) can write to TrustZone enabled registers or features.

It separates your code in a "TrustZone" code and a "user" code. It does not allow your "user code" to access "TrustZone enabled" features, e.g. memory regions, registers.

TrustZone is a "concept" to spit your entire FW system (all the code) into two pieces: TrustZone code or not TrustZone  ("user").
The MCU has registers which can be enabled as "only access-able in TrustZone mode". So, your "user" code cannot modify or do anything (on HW, system, even in memories) when this sits now in "TrustZone".
The MCU would "know" which code is executed as "TrustZone" code and which is not (it realizes the code executed, in which mode or from where it is executed, it "knows" if it is "TrustZone" code doing something on "TrustZone" registers and memories and does not grant access to "user" code to "TrustZone" stuff).

mete
meteAuthor
Senior
Sep 5, 2024 5:58 AM UTC

I know more or less what TrustZone is and how it functions. My question is specifically about what TZEN does. There are non-ST Cortex-M33 MCUs that gives no such option (thus TrustZone is always enabled) and I find it difficult to understand how TrustZone can be disabled in an implementation with TrustZone. So I wonder if it really does disable/remove TrustZone (related hardware) in the core or is it somehow a workaround to make programmer believe there is no TrustZone running when TZEN=0.

mete
meteAuthor
Senior
Sep 5, 2024 6:12 AM UTC

More specifically, Cortex-M33 TRM says this (page 22):

"When the Arm®v8‑M Security Extension is included in the processor, the programmers
model includes two orthogonal security states, Secure state and Non-secure state. When the
Security Extension is implemented, the processor always resets into Secure state. When the
security state is not implemented, the processor resets into Non-secure state. Each security
state includes a set of independent operating modes and supports both privileged and
unprivileged user access. Registers in the System Control Space are banked across Secure
and Non-secure state, with the Non-secure register view available at an aliased address to
Secure state. When the Arm®v8‑M Security Extension is not included in the processor, the
programmers model includes only the Non-secure state."

I do not see a concept of disabling TrustZone here, so if security extensions are implemented, it sounds like it should always be enabled.

BarryWhit
Lead
Sep 5, 2024 6:28 AM UTC

@mete wrote:

I do not see a concept of disabling TrustZone here, so if security extensions are implemented, it sounds like it should always be enabled.


a security guard may always be present at the front gate, but you can instruct them to either check everyone's papers, or let everyone in.

Furthermore, the quote you provided doesn't state that a chip with TrustZone support is always in the secured state. It only states (at most) that upon reset it defaults to the secure state. To the contrary, the quote explicitly says that when hardware implements TrustZone "the programmers model includes two orthogonal security states".

"- If someone's post helped resolve your issue, please thank them by clicking ""Accept as Solution"".- Please post an update with details once you've solved your issue. Your experience may help others."
mete
meteAuthor
Senior
Sep 5, 2024 6:41 AM UTC

Not sure what is the easiest way to implement this, that is why I wonder, there are probably many details that I cannot think of.

Naturally it is not always in the secure state, but there is no concept of "disabling TrustZone", that was my point. The condition in the documents (TRM or ARMv8-M Arch Ref Man) is if TrustZone is implemented or not. So TZEN=0 sounds like it magically removes the TrustZone or Security extension from the implementation.