2025-01-22 01:36 PM - edited 2025-01-22 01:40 PM
There is a STM32G0B1KET6 and a STM32G0B1KET6N available to order.Chapter 7 Ordering information in the datasheet only evaluates to "x = N for “N” product version". I am curious for more information what this means.
Solved! Go to Solution.
2025-01-22 02:31 PM
A hint in Chapter 7 would be usefull.
2025-01-22 02:16 PM
Hi Uwe,
you'll find the details in the data sheet, section 2:
Description
[...] The devices come in packages with 32 to 100 pins. Some packages with low pin count are available in two pinouts (standard and alternative indicated by “N” suffix). Products marked by N suffix are offering VDDIO2 supply and additional UCPD port versus the standard pinout, therefore those are better choice for UCPD/USB applications. [...]
additionally in fig. 6, 7, 9, 10, 11 and in table 12 (columns 2, 4, 7, 8 under Pin Number).
Hope that answers your question?
Regards
/Peter
2025-01-22 02:31 PM
A hint in Chapter 7 would be usefull.