cancel
Showing results for 
Search instead for 
Did you mean: 

What are these in hex file?

-----????_---- ---??as
Associate III
Posted on August 11, 2017 at 14:20

0690X00000607ovQAA.png

When I looked up the stlink utility , I couldnt see 1,2 and 3 shown in the figure?What are these can sb tell me about it?

#hexfile
This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Posted on August 12, 2017 at 08:37

Thanks for your help but I expected to get the value of loaded into Flash in Record Type 05 according to Wiki.I dont get it?The four data byte is => 08000189 What is this?Also How can I record the reset handler in Flash Memory?How will the microcontroller understand that flash memory is reset handler?

Posted on August 12, 2017 at 14:01

It is meta data for the debugger or loader, the CPU uses the value in the vector table already described in the flash content portion.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..