2017-08-11 05:20 AM
When I looked up the stlink utility , I couldnt see 1,2 and 3 shown in the figure?What are these can sb tell me about it?
#hexfileSolved! Go to Solution.
2017-08-12 01:37 AM
Thanks for your help but I expected to get the value of loaded into Flash in Record Type 05 according to Wiki.I dont get it?The four data byte is => 08000189 What is this?Also How can I record the reset handler in Flash Memory?How will the microcontroller understand that flash memory is reset handler?
2017-08-12 07:01 AM
It is meta data for the debugger or loader, the CPU uses the value in the vector table already described in the flash content portion.