cancel
Showing results for 
Search instead for 
Did you mean: 

NUCLEO-C562RE boot0 pin issue

Jean-Guillaume
Visitor

Hi,

I'm currently developing on the NUCLEO board and I can't enter the bootloader using the boot button on the board.

I created an .ioc file with CubeMX2 v1.0.1 using the NUCLEOC562RE board. Then build and flash the code with vscode addon without issue.

When I press the "BOOT" button, perform a "RESET" using the reset button, and then release the "BOOT" button, I continue to boot from the flash memory and therefore cannot access USB DFU mode on USB1, which is my goal ...

However, when I change the value of BOOT0 to 1 in CubeProgrammer using ST-LINK, I can enter USB DFU mode without any issues on USB1. Is it possible to change BOOT0 from the application then ? How ?

Thank you in advance for your help !

0 REPLIES 0