cancel
Showing results for 
Search instead for 
Did you mean: 

What are the differences between Stm32 Nucleo-64 f446Re and Stm32 Nucleo-64 f401Re development boards ?

RSham.1
Associate II

which one is more advantageous to work with as a Student and developer.

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
Imen.D
ST Employee

Hello @RSham.1​ ,

The choice it depends on your needs and on application requirements.

I will recommend to review the STM32F401RE and STM32F446RE Overviews and compare the key features.

Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

The F446RE is a more powerful part.

Consider also using NUCLEO-144 boards, there is better pin escape, and VCP support.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

U mean i terms of clock frequency or any thing else ​too?

I tried but couldn't notic rmuch other than in clock frequency ​.​

The specs were pointed too above

401RE 84 MHZ FLASH:512KB RAM:96KB, TIM:11, U(S)ART:3 ADC:1, DAC:0, CAN:0

446RE 180 MHZ FLASH:512KB RAM:128KB, TIM:17, U(S)ART:6, ADC:3, DAC:2, CAN:2

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..