2019-01-17 5:58 AM
The code works if i enter in stop mode but not if i enter in under drive mode.
I think i have to reinit something after stop mode but i dont find what.
Here is the code :
int main(void)
{
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_ADC1_Init();
MX_RTC_Init();
while (1)
{
HAL_GPIO_WritePin(GPIOB, LED_Pin, GPIO_PIN_RESET);
if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 500, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)
{
Error_Handler();
}
HAL_SuspendTick();
HAL_PWREx_EnterUnderDriveSTOPMode(PWR_LOWPOWERREGULATOR_UNDERDRIVE_ON, PWR_STOPENTRY_WFI); // -200uA
//HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI); // 0.450mA
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
SYSCLKConfig_STOP();
HAL_ResumeTick();
if (HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, 500, RTC_WAKEUPCLOCK_RTCCLK_DIV16) != HAL_OK)
{
Error_Handler();
}
HAL_PWR_EnterSTANDBYMode();
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE3);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.LSIState = RCC_LSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK)
{
Error_Handler();
}
PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_RTC;
PeriphClkInitStruct.RTCClockSelection = RCC_RTCCLKSOURCE_LSI;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
{
Error_Handler();
}
}
void SYSCLKConfig_STOP(void)
{
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
uint32_t pFLatency = 0;
__HAL_RCC_PWR_CLK_ENABLE();
__HAL_RCC_SYSCFG_CLK_ENABLE();
HAL_RCC_GetOscConfig(&RCC_OscInitStruct);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI|RCC_OSCILLATORTYPE_LSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
HAL_RCC_GetClockConfig(&RCC_ClkInitStruct, &pFLatency);
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, pFLatency) != HAL_OK)
{
Error_Handler();
}
}Thanks for your help
Solved! Go to Solution.
2019-01-23 11:37 PM
Hello all,
There is a bug in
HAL_PWREx_EnterUnderDriveSTOPMode(PWR_LOWPOWERREGULATOR_UNDERDRIVE_ON, PWR_STOPENTRY_WFI);
which manipulate the URDY Flag.
It works with underdrive current if you use in place of :
__HAL_PWR_UNDERDRIVE_ENABLE();
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_UNDERDRIVE_ON, PWR_STOPENTRY_WFI);
Perhaps ST can give information about this ?
Thanks,
Thanks,
2019-01-23 11:37 PM
Hello all,
There is a bug in
HAL_PWREx_EnterUnderDriveSTOPMode(PWR_LOWPOWERREGULATOR_UNDERDRIVE_ON, PWR_STOPENTRY_WFI);
which manipulate the URDY Flag.
It works with underdrive current if you use in place of :
__HAL_PWR_UNDERDRIVE_ENABLE();
HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_UNDERDRIVE_ON, PWR_STOPENTRY_WFI);
Perhaps ST can give information about this ?
Thanks,
Thanks,
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.