2008-05-11 09:38 PM
Verify with anglia
2011-05-17 03:34 AM
Hello
I am not sure if this is the right forum for my question. I am using the anglia idealist with the sarm tool-chain. I implemented an addtional section in the linkerscript. Everything works fine. Only the verification after programming the flash fails if i use the additional section. If i just use the standart section verifing is ok. Is it possible to tell the verification tool, that there is a new section?2011-05-17 03:34 AM
Hi sjo
I believe that this is for you :) Cheers, STOne-32.2011-05-17 03:34 AM
???
2011-05-17 03:34 AM
Hi,
What version of the toolchain/ide are you using? Try programming using a different format, eg. binary. and see whether that passes verify. Cheers sjo2011-05-17 03:34 AM
Hi
I am using Angle IDEalist 1.61. If I change to one of the other formats, e.g. Motorola s19, verifing fails too and debugging with these formats doesn't work.2011-05-17 03:34 AM
Post the linker script here, and i will look into it
Cheers sjo