cancel
Showing results for 
Search instead for 
Did you mean: 

Verify with anglia

dschneeweis
Associate II
Posted on May 12, 2008 at 06:38

Verify with anglia

6 REPLIES 6
dschneeweis
Associate II
Posted on May 17, 2011 at 12:34

Hello

I am not sure if this is the right forum for my question.

I am using the anglia idealist with the sarm tool-chain. I implemented an addtional section in the linkerscript. Everything works fine. Only the verification after programming the flash fails if i use the additional section. If i just use the standart section verifing is ok.

Is it possible to tell the verification tool, that there is a new section?

16-32micros
Associate III
Posted on May 17, 2011 at 12:34

Hi sjo

I believe that this is for you :)

Cheers,

STOne-32.

dschneeweis
Associate II
Posted on May 17, 2011 at 12:34

???

sjo
Associate II
Posted on May 17, 2011 at 12:34

Hi,

What version of the toolchain/ide are you using?

Try programming using a different format, eg. binary. and see whether that passes verify.

Cheers

sjo

dschneeweis
Associate II
Posted on May 17, 2011 at 12:34

Hi

I am using Angle IDEalist 1.61.

If I change to one of the other formats, e.g. Motorola s19, verifing fails too and debugging with these formats doesn't work.

sjo
Associate II
Posted on May 17, 2011 at 12:34

Post the linker script here, and i will look into it

Cheers

sjo