Using Vbat as ADC for battery level monitoring
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-26 8:18 PM
I'm updating an old PCB design that used the STM32L432KB. The new design is using the STM32L452CE which has the Vbat pin.
In the old design I used a voltage divider across the battery and connected it to an ADC pin to periodically check the battery level.
In the new design instead of using a voltage divider to an ADC pin can I use a connection from the positive terminal of the battery straight to the Vbat pin?
I don't wish to use Vbat as a backup power supply or any of the other feature, just as an ADC input since the board is to be powered with the battery only.
#adc #vbat #battery-life #battery- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-26 9:05 PM
In the new design instead of using a voltage divider to an ADC pin can I use a connection from the positive terminal of the battery straight to the Vbat pin?
Yes. Possible.
Below is the image snapshot from
of the MCU.Couple of points:
- Enable the bridge (CH18SEL) only during measurement. else it will drain battery continuously.
- The read analog value represents will be one third of the actual battery voltage.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-26 11:33 PM
Check the normal operating input voltage of vbat to make sure weather the battery can be direct connect to vbat pin or not. As i recall, the adc will have an inyernal divider to scale the voltage within mid range of the adc. It has a power switch to reduce leakage. Using vref adc channel, the accurate vbat voltage can be calculated properly.
If the vbat is 5v, it would probably require an external divider...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-07-28 1:33 AM
If the battery is 4.6V, the vbat gpio maynot be 5v tolerant, hence make sure not to beleive 5/3 will solve it...