cancel
Showing results for 
Search instead for 
Did you mean: 

Using PC_1 and PC_5 results in a faulty reading values, Why?

MJala.8
Associate

The question is regarding Nucleo-l476RG, I need to use 5 ADC, 12Bit.

No matter what I do. I cannot see that these pins are connected to anything else.

Why do I get a wrong reading on these GPIO?

Please notice that my board is new .. the MCU is not damaged.

I used the PB_1 for the same measurements and it works just fine. I have no idea why this happens.

I use mbed-os in my project .. I don't think it is mbed-os's fault either.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Check solder-bridge options for PC1

https://www.st.com/content/ccc/resource/technical/document/user_manual/98/2e/fa/4b/e0/82/43/b7/DM00105823.pdf/files/DM00105823.pdf/jcr:content/translations/en.DM00105823.pdf

If it is not hardware, then it is software. Proof the design using HAL, LL or register level code. Probe the pin-to-pin with a meter.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
MJala.8
Associate

HW was OK.

And why should the mbed not work just for these two pins? I don't get that.

The value reads from these pins seems to be multiplied by factor > 1.5

The same software I used with PB_1 and it works just fine.

Don't know what could cause that.