Using MCO (Master Clock Out) as I2S MCLK
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-07-12 8:03 AM
Posted on July 12, 2015 at 17:03
Hello,
I'm currently working on simple device, which main task would be collecting data from ADC (via i2s) and sending them to base station via wireless (SPI based) transceiver.I'm planing to use STM32F103RCT6/8 series MCU.However it operates on so low clock and doesn't have I2SPLL module that I would be unable to provide MCLK signal for ADC/DAC on I2S. Is it possible to use MCO (Master Clock Output) signal, setup to 36MHz? Also would I2S slave SCK be in synch with this MCO signal as required by ADC?''Please note there is no required phase relationship, but MCLK, LRCK andSCLK must be synchronous.''Thank You for supportChris #i2s #stm32f1 #mco
Labels:
- Labels:
-
I2S
-
STM32F1 Series
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-07-12 9:35 AM
Posted on July 12, 2015 at 18:35
Can you output 36 MHz, Yes PLL/2
Will slaves to the same 36 MHz clock be synchronous, Yes.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..