2014-01-14 7:46 PM
Hi. Is it possible to setup EXTI_LineX so that it is only triggered by EXTI_GenerateSWInterrupt(EXTI_Linex) library function? and NOT triggered by any hardware condition?
It seems that even if I omit the code for linking GPIO_PORT to EXTI_Line, it automatically links EXTI_Line to GPIOA. GPIOA happen to have SPI clock, which I think is triggering EXTI interrupt on every falling edge.Anyone have idea??Thank you #exti