Question
Using BDMA2 on a timer to control a GPIO port using a STM32H7
I feel that CubeMx and HAL will reveal no solution to this but I still would like a solution to this problem. The GPIO pins on the H7 are on the AHB4 bus, as is BDMA2. I wish to set a timer to cycle through a buffer toggling a GPIO port outputs. Is this even possible? I've had good result using BDMA on DAC2 so I'm aware of the 32Kb in the SRD RAM and understand that this will be the only memory addressable...