2015-10-16 6:34 AM
Hello,
A bit of a beginner question here. I want to have a timer interrupt to trigger every x mS. This is the code I've made so far but it's not triggering any interrupt. int uwPrescalerValue = (uint32_t) ((SystemCoreClock /2) / 10000) - 1; htim3.Instance = TIM3; htim3.Init.Prescaler = uwPrescalerValue; htim3.Init.CounterMode = TIM_COUNTERMODE_UP; htim3.Init.Period = 100; htim3.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; if(HAL_TIM_Base_Init(&htim3) != HAL_OK) { while(1) { } } if(HAL_TIM_Base_Start_IT(&htim3) != HAL_OK) { while(1) { } } __HAL_RCC_TIM3_CLK_ENABLE(); /* Set the TIMx priority */ HAL_NVIC_SetPriority(TIM3_IRQn, 0, 1); /* Enable the TIMx global Interrupt */ HAL_NVIC_EnableIRQ(TIM3_IRQn); Am I missing something to enable the timer interrupt here? Best regards, Rik