cancel
Showing results for 
Search instead for 
Did you mean: 

Use a 14.7456MHz crystal with STM32G031 (32PIN) IO-Link application

MGons.1
Associate II

Hi is it possible to use a 14.7456MHz crystal with a STM32G031 (LQFP32). If I'm right it is not possible at the data sheet, there is no OSC_OUT for this package. Or is the option missing in the data sheet? We need this crystal for an IO-Link application.

Br Maurice

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @MGons.1​, to the community!

as you have correctly noticed, the STM32G31 does not have an OSC_OUT in packages with less than 48 pins, so only an external oscillator can be used for HSE there. The more powerful brothers STM32G041 and STM32G071 have the same limitation, so you should either switch to a package with more than 32 pins or use an external oscillator circuitry for the 14.7456MHz crystal.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @MGons.1​, to the community!

as you have correctly noticed, the STM32G31 does not have an OSC_OUT in packages with less than 48 pins, so only an external oscillator can be used for HSE there. The more powerful brothers STM32G041 and STM32G071 have the same limitation, so you should either switch to a package with more than 32 pins or use an external oscillator circuitry for the 14.7456MHz crystal.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.