cancel
Showing results for 
Search instead for 
Did you mean: 

USB1.0

HT
Associate

Hi,

I using Eval boar : stm3210E-eval (stm32F103ZG6)

I want to communicate with an external device vua USB, this device should be communicatre with USB1 gen,

I ask if it could be with this eval board?>

If not, if I use this MCU stm32f103ZG6 and make a private PCB, can I communicate with external device with USB1.0?

 

HMT

 

1 REPLY 1
Issamos
Lead II

Hello @HT 

Sens the eval board comes with a USB 2.0 than it can communicate with  USB 1.0

Best regards.

II