USB SOF PIN?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-04-25 12:06 AM
Posted on April 25, 2014 at 09:06
A section of code in the USB host lib 2.0 has been puzzling me for some time now, it is within the USB_OTG_BSP_Init function:
/* Configure SOF Pin.*/ // GPIO_InitStructure.GPIO_Pin = HOST_OVRCURR_LINE; // GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; // GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IPU; // GPIO_Init(HOST_OVRCURR_PORT, &GPIO_InitStructure); I've commented the code and everything's running OK (so far) but I don't want loose ends in my codes so I'm here to ask if anyone could tell me what does it do? From my very primitive and limited understanding of USB protocol, it has something to do with Start of Frame packet, but what is a SOF ''pin''? Isn't SOF packet sent using NRZI coding using just one line DM/DP? (not counting VBUS and GND)
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0