Posted on May 17, 2011 at 14:34 Sorry for posting here ; but still I cant open a new thread ! hope someone from sT help me.
My subject:
I used STM32F103 and 105 in some small projects before; it is just good mcu.
now I need to add to my boards a USB host to interface with usb flash stick inorder to save some data as txt files .
is 105 is ok do to this ? or should i go with 107?
is there a library or example to try it iorder to create a txt file and write data in it .
I want to use A usb conenctor ; so I have can only connect DM and DP ; i will not use ID pin ; is that important as a host usb ?
any examples and guides would great .
Thanks is advanced and sorry for posting here ; I hope the moderators see my thread and help me to solve the problem.
Regards