2009-09-24 08:53 AM
USB iap about connectivity line
2011-05-17 04:24 AM
usb iap for stm32f103x is ok.
but can not work under connectivity line. can anyone share the connectivity line usb iap examples? thanks in advance.2011-05-17 04:24 AM
Quote:
usb iap can not work under connectivity line.
What makes you say that?2011-05-17 04:24 AM
Try the system boot mode, the DFU is implemented on Connectivity line natively ;-)
On other hand, the standard USB drivers from 103 don't work on 105/107, the device lib should be released till eof September.