USB: how to increase the input and output receive buffer
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-12-02 12:24 PM
Posted on December 02, 2014 at 21:24
Hello,
I designed my own application starting from VirtualComport_loopback example project.I have a modbus client protocol running on USB and using CDC_Send_DATA() and CDC_Receive_DATA() send and get data from PC virtual comm. port.I have problems with modbus commands with read and/or writes longer that 64 bytes. I resolved the output problem splitting the answer into 64 bytes blocks. I wonder if I can do the same thing with input or increase the input buffer to 256 bytes (max. protocol message length).Here is some piece of code:uint32_t CDC_Send_DATA (uint8_t *ptrBuffer, uint16_t Send_length){ uint8_t len; uint8_t *buff = ptrBuffer; packet_sent = 0; while (Send_length) { if (Send_length < 64) len = Send_length; else len = 64; /* send packet to PMA*/ UserToPMABufferCopy((unsigned char*)buff, ENDP1_TXADDR, len); SetEPTxCount(ENDP1, len); SetEPTxValid(ENDP1); Send_length -= len; buff += len; Delay_10ms(2); } return 1;}
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0