USB Host example on STM32F7 (or STM32Fx) without class-driver?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2015-08-07 1:22 AM
Posted on August 07, 2015 at 10:22
Hi,
Is there any USB host example without class-specific driver? I see some examples in the Cube lib, but all are class-specific eg HID/MSC/etcI would like to have a 'direct' comms between a F7-disco and an external USB device via plain usb endpoints.So, I have to see how to communicate from a host application to the external device via usb pipes/endpoints.Is there something that I can have as an example project for that?RegardsChristos
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0