cancel
Showing results for 
Search instead for 
Did you mean: 

USB Host does not detect flashdisk plugin and no interrupt occurrence

runbaby
Associate

I am use Nucleo-H563Zi test the usb host feature, I connected the USB_USER jumper to provide VBUS, and just use 2 wire usb, ignore 2 CC line. and configed in cubeide as below

runbaby_0-1702702131240.pngrunbaby_1-1702702155126.pngrunbaby_2-1702702189393.png

runbaby_3-1702702226922.png

Then I generat code, and I add 

"HAL_HCD_Start(&hhcd_USB_DRD_FS);"

before while(1)

 

then compile and debug the program

but I can not detect the flash disk plugin and no usb interrupt occure.

what config is wrong for this test.

 

Thank you.

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
runbaby
Associate

find the reason, we need enable USB33SV in register PWR_USBSCR, and this implement in HAL_PWREx_EnableVddUSB(), and was not generate by cubeide,  we need add this function call manually,

after that it works good.

View solution in original post

1 REPLY 1
runbaby
Associate

find the reason, we need enable USB33SV in register PWR_USBSCR, and this implement in HAL_PWREx_EnableVddUSB(), and was not generate by cubeide,  we need add this function call manually,

after that it works good.