2015-04-13 7:51 PM
I am developing a HID USB with STM32F107, and iam currently using STM32_USB-FS-Device_Lib_V4.0.0.
1. My problem is that i dont understand clearly about USB_DISCONNECT feature in this MCU.2. I see in the library, ST define some GPIO for USB disconnect#if defined(STM32L1XX_MD) || defined(STM32L1XX_HD)|| defined(STM32L1XX_MD_PLUS)|| defined(STM32F37X)|| defined(STM32F30X) /* Enable the SYSCFG module clock (used for the USB disconnect feature) */ RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);and /* Define the STM32F10x hardware depending on the used evaluation board */#ifdef USE_STM3210B_EVAL #define USB_DISCONNECT GPIOD #define USB_DISCONNECT_PIN GPIO_Pin_9 #define RCC_APB2Periph_GPIO_DISCONNECT RCC_APB2Periph_GPIOD #define RCC_APB2Periph_ALLGPIO (RCC_APB2Periph_GPIOA \ | RCC_APB2Periph_GPIOB \ | RCC_APB2Periph_GPIOC \ | RCC_APB2Periph_GPIOD \ | RCC_APB2Periph_GPIOE )It seems that different boards have different pin configuration for USB disconnect.So, how can i know which GPIO pin is USB Disconnect in my MCU.3. Difference between internal USB pullup vs external USB pullup