cancel
Showing results for 
Search instead for 
Did you mean: 

USB device troubles, setup packet Cancelled

Georg Doza
Associate II
Posted on May 28, 2015 at 17:47

When i developing custom USB device, I vent into trouble and at end I isolated a problem:

First: USB device answer for this packet is ''Success''

  

Setup Packet

Offset Field Size Value Description

0 bmRequestType 1 23h

4..0: Recipient ...00011  Other

6..5: Type .01.....  Class

7: Direction 0.......  Host-to-Device

1 bRequest 1 01h

2 wValue 2 0014h

4 wIndex 2 0001h

6 wLength 2 0000h

Second: and answer to following packet is ''Cancelled''

Setup Packet

Offset Field Size Value Description

0 bmRequestType 1 40h

4..0: Recipient ...00000  Device

6..5: Type .10.....  Vendor

7: Direction 0.......  Host-to-Device

1 bRequest 1 04h

2 wValue 2 0207h

4 wIndex 2 0000h

6 wLength 2 0000h

What cause different reaction of an USB device?

Framework is the USB_OTG_library, F407 processor, USBluzer sniffer.

GeorgD
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0