2013-02-25 02:52 PM
Hello,
Can someone inform me whether I can use (or do I need) USB CDC Driver on Windows CE. I am planning to connect STM32F4 Discovery to Cuwin Touch Screen panel which is operated on Windows CE. I checked the 'readme' file which comes with the driver and it says it is only compatible with Windows 98 SE, 2000, XP, Vista, 7. Thanks for the help2013-02-25 03:33 PM
WinCE is NOT compatible with drivers from those other Microsoft operating systems, and in many cased doesn't even use an x86 CPU.