2010-12-17 1:53 AM
USART1 & TIM1 working parallel ?
2011-05-17 5:18 AM
''Is there a known reason why my first initialization example not works''
Take a look at the spreadsheet here:[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/STM32VL Discovery Kit Global Pinouts View&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000491D59B8574F8049B5DFA3E8B21CBA51&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/AllItems.aspx¤tviews=382]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32VLDiscovery/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fSTM32VLDiscovery%2fSTM32VL%20Discovery%20Kit%20Global%20Pinouts%20View&FolderCTID=0x01200200770978C69A1141439FE559EB459D758000491D59B8574F8049B5DFA3E8B21CBA51&TopicsView=https%3A%2F%2Fmy%2Est%2Ecom%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32VLDiscovery%2FAllItems%2Easpx¤tviews=382 It shows you the full pinout, and what functions are shared on pins...''have I to check my code ?''Yes, of course you do!
2011-05-17 5:18 AM
Thank you, I know this fine spreadsheet.
My question was if I use TIM1_CH1 at PA8 that damage my USART1 or not. And why using TIM1_CH4 don't do that. The source for using CH1 or CH4 is nearly the same. Have I reconfigure the USART1 for that ?2011-05-17 5:18 AM
After checking the TIM1 register against the manual I saw a false value
in the TIM1->CCER register in case I use TIM1-CH1. I've forgotton the struct initialization TIM_OCStructInit (&TIM_OCInitStructure) After that everything is fine. Thank you for pointing me in the right direction.