cancel
Showing results for 
Search instead for 
Did you mean: 

USART1 doesn't work

Arnas Matiukas
Associate II
Posted on February 11, 2018 at 15:00

Hello everyone. I have encountered problem with USART1 on STM32F446RE. It seems it doesn't work for me. I have used multiple times USART2 and it works as it should, but USART1 with same configurations just refuse to work. What could be the problem?

I use STM32CubeMX v4.24.0.

UART_HandleTypeDef huart1;

UART_HandleTypeDef huart2;

void SystemClock_Config(void);

static void MX_GPIO_Init(void);

static void MX_USART1_UART_Init(void);

static void MX_USART2_UART_Init(void);

int main(void)

{

   HAL_Init();

   SystemClock_Config();

   MX_GPIO_Init();

   MX_USART1_UART_Init();

   MX_USART2_UART_Init();

   while (1)

   {

      HAL_UART_Transmit_IT(&huart1, (uint8_t *)'Hello with USART1\r\n', strlen('Hello with USART1\r\n'));

      HAL_Delay(1000);

      HAL_UART_Transmit_IT(&huart2, (uint8_t *)'Hello with USART2\r\n', strlen('Hello with USART2\r\n'));

   }

}

static void MX_USART1_UART_Init(void)

{

   huart1.Instance = USART1;

   huart1.Init.BaudRate = 115200;

   huart1.Init.WordLength = UART_WORDLENGTH_8B;

   huart1.Init.StopBits = UART_STOPBITS_1;

   huart1.Init.Parity = UART_PARITY_NONE;

   huart1.Init.Mode = UART_MODE_TX_RX;

   huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;

   huart1.Init.OverSampling = UART_OVERSAMPLING_16;

   if (HAL_UART_Init(&huart1) != HAL_OK)

   {

      _Error_Handler(__FILE__, __LINE__);

   }

}

static void MX_USART2_UART_Init(void)

{

   huart2.Instance = USART2;

   huart2.Init.BaudRate = 115200;

   huart2.Init.WordLength = UART_WORDLENGTH_8B;

   huart2.Init.StopBits = UART_STOPBITS_1;

   huart2.Init.Parity = UART_PARITY_NONE;

   huart2.Init.Mode = UART_MODE_TX_RX;

   huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;

   huart2.Init.OverSampling = UART_OVERSAMPLING_16;

   if (HAL_UART_Init(&huart2) != HAL_OK)

   {

      _Error_Handler(__FILE__, __LINE__);

   }

}

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Posted on February 11, 2018 at 18:20

Thank you for clarification !