2015-01-27 07:05 AM
Hello,
is it possible to use one USART in HalfDuplexMode (Rx and Tx via Tx Pin) AND the Rx Pin of the same USART to receive another stream? regards Florian2015-01-27 08:13 AM
is it possible to use one USART in HalfDuplexMode (Rx and Tx via Tx Pin) AND the Rx Pin of the same USART to receive another stream?
Some how I think it would be very hard to manage, and not lose data.2015-01-28 12:04 AM
Hello Clive,
thank you for the information. regards Florian