2016-10-12 11:40 PM
2016-10-13 08:34 AM
Code appears incomplete, attach as a file, or use the Format Source Code tool (Paintbrush [< >] icon)
If the message keeps concatenating, then you need to clear or reset the string after each output.The IRQ Handler would need to call into the HAL for the callbacks to be serviced. Unfortunately I can't provide support for HAL based code.2016-10-18 08:58 PM
Hi Clive,
Thanks for the reply.Can you just suggest me some links which will provide the codes for the task.It will be truly helpful if you could suggest some as I am finding it difficult to do it myself alone without any guidance from anyone. Regards Anjana2016-10-19 07:56 AM
HAL isn't my thing, I've provided many SPL examples
The CubeMX install should provide a number of examples that might be useful to reviewSTM32Cube_FW_F1_V1.3.0\Projects\STM3210C_EVAL\Examples\UART