cancel
Showing results for 
Search instead for 
Did you mean: 

Uploading new firmware (AN2606)

johan239955_st
Associate II
Posted on June 25, 2009 at 02:01

Uploading new firmware (AN2606)

4 REPLIES 4
johan239955_st
Associate II
Posted on May 17, 2011 at 13:14

The firmware in my application shall be able to upgrade over USART1 as described in AN2606. However, using the windows application written by ST is almost impossible since it does not really coop with the USB-to-serial converters that I'm are using.

I have earlier been using mcuisp, which successfully uses the USB-to-serial converters, but the problem is that mcuisp erases all flash before new firmware is downloaded to the device. This means that it erases a parameter area that must not be erased.

Do you have any suggestions on how to upload new FW without destroying the parameter area?

alex8
Associate II
Posted on May 17, 2011 at 13:14

Maybe what would help you most would be if people here could advise as to what specific model USB-serial converters they are successfully using with the ST software?

I'd make sure you've got the most up to date drivers for whatever usb-serial pod you've got.

If you've got a Linux running somewhere, you could give my

http://sourceforge.net/projects/sloadhost/

project a shot. :) It implements the page-by-page erase function of AN2606. I'm working on a Windows port for this, but don't know when it'll be ready.

Cheers,

Alex

alex8
Associate II
Posted on May 17, 2011 at 13:14

Hello Johann,

I've got a windows version of Sloadhost working now... at least on my machine.

The format for a limited pages erase would be

sloadhost-stm32.exe --serialdev com1 --baudrate 57600 --pageserase 0,1,2,3

to erase the first 4 pages, if the uC is in it's AN2606 bootloader mode.

As long as protection isn't set, you do not need to do a global erase.

Alex

mcuisp
Associate II
Posted on May 17, 2011 at 13:14

Hi johan:

Before Start isp download,the mcuisp.exe will Erase All, because this is need to disable ReadOutProtection.

I suggest you to use the FreeIAP, come with mcuisp.exe. This IAP will just erase the sector which need to reprogram, and reserve the parameter FLASH you used.

The FreeIAP will use the first 4KB FLASH. and use USART0 also. it is useful when debug program.

Hope this will be helpful to you.

James,www.McuIsp.com

mailto:McuIsp@gmail.com