cancel
Showing results for 
Search instead for 
Did you mean: 

Unstable logical state on every I/O pin

ProgBoy
Associate

Hi Everybody! 

I confronts a very interesting problem at my project. Details above:

Hardware: NUCLEOG071RB

Attached the IOC configuration. Control the SPI CS pin by software. I got small 4-8us signal spikes all  GPIO, SPI, I2S pins. SPI and I2S powered by DMA. 

I tried connect serially 33K resistor with less success. The 3.3V power line is stable. Jumper wire length 10 cm. 

Any idea what I did wrong? pics2.png

 

pics1.png

 

2 REPLIES 2
AScha.3
Chief III

Hi,

>Any idea what I did wrong? 

How about your ground connections ? (spikes on all lines = typical for bad/long/indirect ground connection)

If you feel a post has answered your question, please click "Accept as Solution".
TDK
Guru

Looks like all glitches are positive-going pulses. Is your logic level set to 3.3 V and not 1.65 V? You can filter out glitches on each channel.

If you feel a post has answered your question, please click "Accept as Solution".