cancel
Showing results for 
Search instead for 
Did you mean: 

Understanding FSMC arbitration

sk-st
Associate III
Posted on September 22, 2014 at 12:38

I want to direct drive a rgb tft display via FSMC/DMA and an external async sram as framebuffer. The cpu is a STM32F103ZC.

What happens when CPU writes between transfers to RAM?

The transfers would be then: DMA Read (FSMC SRAM), DMA Write (FSMC TFT), CPU Write (FSMC SRAM).

I have read that there is a round robin scheduler. How much bandwidth can CPU get in this case?
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
waclawek.jan
Super User
Posted on September 22, 2014 at 13:03

You should read AN2548. Beyond what's given there, you are left to experimentation, I am afraid.

JW