2025-03-28 7:03 AM - last edited on 2025-03-28 7:06 AM by Andrew Neil
Hello,
I would like some advice on understanding a code with an example provided with the STM32L5xx evaluation board. I have this code below :
/* Initialize the data buffer */
for(int i=0; i < PLAY_BUFF_SIZE; i+=2)
{
PlayBuff[i]=*((__IO uint16_t *)(AUDIO_FILE_ADDRESS + PLAY_HEADER + i));
}PLAY_BUFF_SIZE = 4096
uint16_t PlayBuff [PLAY_BUFF_SIZE];
#define AUDIO_FILE_ADDRESS 0x08040000
#define PLAY_HEADER 0x2C
I understand a little bit but where does the value 0x2C come from, what does it come from ? What does PLAY_HEADER mean ?
Thank you for your helps.
Solved! Go to Solution.
2025-03-28 7:28 AM
The WAV file has a 44-byte header. This skips past the header and reads the data.
2025-03-28 7:28 AM
The WAV file has a 44-byte header. This skips past the header and reads the data.
2025-03-28 7:36 AM
@TDK wrote:The WAV file has a 44-byte header. This skips past the header and reads the data.
Where did you find this information ? Indeed, at the beginning it says that you have to load the music into a memory area.
2025-03-28 7:40 AM
WAV is a well-known, standard file format - it is well documented; eg,
https://en.wikipedia.org/wiki/WAV#WAV_file_header
2025-03-28 7:54 AM - edited 2025-03-28 7:54 AM
I searched google and also have general knowledge that files often have a header which lines up with the variable names.
2025-03-28 8:17 AM - edited 2025-03-28 9:33 AM
@TDK wrote:I searched google and also have general knowledge that files often have a header which lines up with the variable names.
Thank you for this information, I can often see audio but nothing tells me that it is the WAV format but apparently it is the case. So if I understand correctly, we make a copy of the data recorded at the AUDIO_FILE_ADDRESS address
in the PlayBuff table ? why is the size 4096 ?
Isn't this size chosen randomly ? It depends on the SAI speed and the frame length to go fast enough so as not to lose data in the DMA. Right ?
2025-03-28 12:59 PM
> So if I understand correctly, we make a copy of the data recorded at the AUDIO_FILE_ADDRESS address
in the PlayBuff table ?
Yes.
> why is the size 4096 ?
Yes, 4096 is somewhat arbitrary. It should be large enough that you only need to update it every 1ms or more, but small enough to fit into memory.