2022-04-21 6:01 AM
Hello all
I have a custom STM32L496RGT3 based board which I've configure to run at 64MHz off the HSI using CubeIDE:
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct = {0};
RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};
/** Configure the main internal regulator output voltage
*/
if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
{
Error_Handler();
}
/** Initializes the RCC Oscillators according to the specified parameters
* in the RCC_OscInitTypeDef structure.
*/
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 1;
RCC_OscInitStruct.PLL.PLLN = 8;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2;
RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2;
if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
{
Error_Handler();
}
/** Initializes the CPU, AHB and APB buses clocks
*/
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
|RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3) != HAL_OK)
{
Error_Handler();
}
}I'm getting some very strange behaviour though: on some boards my firmware runs fine, on others it fails quite early - usually in some banal non-pointer related code (there's actually no pointers or arrays anywhere in the code) - jumping off outside the program to address 0x1fff093e. I get the get the same behaviour running from the debugger, but not if I single step through the code.
I was wondering if there's any special flash latency - or anything else - set up required?
2022-04-21 8:41 AM
You can increase flash latency to see if that fixes it. Doubt it will.
When it's outside of program code, what does the call stack look like?
Sounds like a hardware issue. Is VDD stable? VCAP sufficient and stable? Can you monitor NRST line to see if issue corresponds to an NRST pulse?
2022-04-21 8:44 AM
I just tracked the problem down.
Running on a 1,2V lab power supply everything's fine. It turns out that some of the batteries are a little bit border-line in terms of charge, and it's only those ones that fail.
The symptoms seem a little strange, but I'm putting the whole thing down to a weedy power supply.
2022-04-21 8:45 AM
Make sure your design pulls BOOT0 LOW
That SCB->VTOR maps to your code base in FLASH
After programming flash, power cycle the board
2022-04-21 8:55 AM
It will go into the ROM if the state of BOOT0 is indeterminate at reset, ie looks to float high rather than low, with a sketchy supply, or one rising slowly.