Skip to main content
urgentmeow
Associate
November 17, 2020
Solved

Unable to set up the FMC for 16-bit writes; always sends 64 bits (STM32H753I-eval2)

  • November 17, 2020
  • 2 replies
  • 1883 views

I'm trying to configure Bank 1 of the FMC in Mode 1 (SRAM). I'm nearly there but ran into a frustrating problem, where it insisted on writing 64 bytes despite me setting the FMC's MWID register to 01 (16 bits) and using a uint16_t* in C to perform the write. The reference manual mentions an AXI bus width of 64 bits, and seems to imply that it's configurable somewhere, but I can't find where that might be. On an oscilloscope, I can see that when I try to perform a 16-bit write, chip select goes high and there are four write strobes. If I set MWID to 8 bits, there are eight write strobes. MWID to 32 bits gives two write strobes. Where else besides the BTCR register do I need to configure the FMC's bus width?

Here's my configuration, for reference:

 // Zero out all the bits we want to configure (or to be zero)
 FMC_Bank1_R->BTCR[0] &= ~(
 FMC_BCR1_FMCEN |
 FMC_BCR1_BMAP |
 FMC_BCR1_WFDIS |
 FMC_BCR1_CCLKEN |
 FMC_BCRx_CBURSTRW |
 FMC_BCRx_CPSIZE |
 FMC_BCRx_ASYNCWAIT |
 FMC_BCRx_EXTMOD |
 FMC_BCRx_WAITEN |
 FMC_BCRx_WREN |
 FMC_BCRx_BURSTEN |
 FMC_BCRx_FACCEN |
 FMC_BCRx_MWID |
 FMC_BCRx_MTYP |
 FMC_BCRx_MUXEN |
 FMC_BCRx_MBKEN
 );
 
 // Set the bits we want to be non-zero.
 FMC_Bank1_R->BTCR[0] |= (
 FMC_BCR1_FMCEN | // Enable memory bank 1
 FMC_BCRx_MBKEN | // Enable FMC
 FMC_BCRx_WREN | // Enable writes
 (1 << FMC_BCRx_MWID_Pos) // Set bus width to 16 bits
 );

Here's how I'm performing the write:

uint16_t* control_port = (uint16_t*) 0x60000000;
uint16_t data = 0x1234;
control_port[0] = data;

This topic has been closed for replies.
Best answer by waclawek.jan

In MPU, set the FMC address range as Device.

JW

2 replies

waclawek.jan
waclawek.janBest answer
Super User
November 17, 2020

In MPU, set the FMC address range as Device.

JW

urgentmeow
Associate
November 17, 2020

Aha, thanks! That seems to be it. For anyone else with the same issue, see this thread.