cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to receive CAN data

ebommer
Associate II
Posted on September 08, 2014 at 23:47

I am working on the STM32F302 Micro and I currently unable to receive data on the CAN bus, I have a break point set on the interrupt routine.  I am able to transmit data.  I am seeing the micro sends an acknowledge bit when I send data from my CAN tool, so I know the message is getting there, but when I look at the receive buffer I see nothing.  I figure since my CAN tool receives the data from the micro without error I have all the timing set appropriately.

I am set for interrupt on Tx and Rx:

    /*  Transmit */

    HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_0);

    HAL_NVIC_SetPriority(USB_HP_CAN_TX_IRQn, 0, 0);

    HAL_NVIC_EnableIRQ(USB_HP_CAN_TX_IRQn);

    /*  Receive */

    HAL_NVIC_SetPriorityGrouping(NVIC_PRIORITYGROUP_0);

    HAL_NVIC_SetPriority(USB_LP_CAN_RX0_IRQn, 0, 0);

    HAL_NVIC_EnableIRQ(USB_LP_CAN_RX0_IRQn);

Interrupt routine:

void USB_LP_CAN_RX0_IRQHandler(void)

{

  HAL_NVIC_ClearPendingIRQ(USB_LP_CAN_RX0_IRQn);

  HAL_CAN_IRQHandler(&hcan);

}

I have F0R1 and F0R2 set to 0x04, I am using an extended ID.

I have CAN transmitting and receiving on a STM32F103 and I have compared my setup and see no difference.  So I am running out of guesses.

#can #bxcan #filter #stm32 #stm32f2 #code #example #stm32-can
This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
rm239955
Associate II
Posted on January 26, 2015 at 15:42

Dear ebommer

Have you found out the solution for this..

Even I am also facing the same problem