2015-04-13 6:56 AM
Help! I have loaded the STM322xG_EVAL/Applications/FreeRTOS/FreeRTOS_LowPower demo project into my STM3220G-EVAL board. Every 500 msec the red LED flashes to show me that the CPU is waking from sleep but I am having trouble reflashing the board since the CPU keeps going to sleep. I am using IAR embedded workbench with an I-jet debugger. Any hints how to accomplish this?
-Scott2015-04-13 10:10 AM
Try strapping BOOT0 High. It will boot the System Loader ROM, not broken code you have downloaded.
See if there are connection options with the I-Jet, like ''connect under reset'', ''Enable debug in low power mode'' or similar.