cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to download and debug flash

milan
Associate II
Posted on October 11, 2010 at 17:28

Unable to download and debug flash

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
Posted on May 17, 2011 at 14:10

You sure it's using 5.50? ''Embedded Workbench 5.4_2''

I haven't bothered with IAR/EWARM, but the Keil 4.12 demo is working with the discovery board.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
milan
Associate II
Posted on May 17, 2011 at 14:10

I don't know why but in uVision 4 i get this message in build output

Build target 'DISCOVER'

compiling system_stm32f10x.c...

compiling core_cm3.c...

assembling startup_stm32f10x_md_vl.s...

compiling stm32f10x_pwr.c...

compiling stm32f10x_rcc.c...

compiling misc.c...

compiling stm32f10x_exti.c...

compiling stm32f10x_gpio.c...

compiling STM32vldiscovery.c...

compiling stm32f10x_it.c...

compiling main.c...

linking...

Program Size: Code=1628 RO-data=348 RW-data=52 ZI-data=1028 

''.\Debug\DISCOVER.axf'' - 0 Error(s), 0 Warning(s).

Load ''D:\\Project\\Project\\Demo\\MDK-ARM\\Debug\\DISCOVER.AXF''

Load ''D:\\Project\\Project\\Demo\\MDK-ARM\\Debug\\DISCOVER.AXF''

but it does't flash the MCU do you know why?

gdoura.marwa
Associate II
Posted on May 17, 2011 at 14:10

Hi,

 

 

This is a known bug in EWARM 5.50  with value line flashloader. It is fixed in EWARM5.50.5.

 

I advise you, if possible, to upgrade your EWARM version to 5.50.5 (available on IAR web site: www.iar.com).

 

 

Else , you can use the attached patch to fix this problem with your installed version. It contains a readme that explains hosw to use it.

 

 

Hope this helps,

 

regards,

VLINE.

Posted on May 17, 2011 at 14:10

I don't know why but in uVision 4 i get this message in build output

 

 

Build target 'DISCOVER'

 

compiling system_stm32f10x.c...

 

compiling core_cm3.c...

 

assembling startup_stm32f10x_md_vl.s...

 

compiling stm32f10x_pwr.c...

 

compiling stm32f10x_rcc.c...

 

compiling misc.c...

 

compiling stm32f10x_exti.c...

 

compiling stm32f10x_gpio.c...

 

compiling STM32vldiscovery.c...

 

compiling stm32f10x_it.c...

 

compiling main.c...

 

linking...

 

Program Size: Code=1628 RO-data=348 RW-data=52 ZI-data=1028 

 

''.\Debug\DISCOVER.axf'' - 0 Error(s), 0 Warning(s).

 

Load ''D:\\Project\\Project\\Demo\\MDK-ARM\\Debug\\DISCOVER.AXF''

 

Load ''D:\\Project\\Project\\Demo\\MDK-ARM\\Debug\\DISCOVER.AXF''

 

 

but it does't flash the MCU do you know why?

LOAD means it sent it to the device. There is a problem with the ST-LINK using the Flash->Download menu, but if you select Debug->Start/Stop and you have enabled ''Update Target before Debugging'' option, it will flash the device before it starts debugging.

If you want to write a specific .HEX file to the device, you can download and use the ST-LINK Utility program outside of Keil.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
nanayakkaraan
Associate II
Posted on May 17, 2011 at 14:11

Hello,

Having the same problem flash loader.

If possible let me have the patch in .zip format. I dont have rar in my machines.

Also I couldnot find the exact place where I can download EWARM version to 5.50.5. Is it freely available?

Now I am using IAR Enbedded workbench 5.4 kickstart.

Thank you.

nanayakkaraan
Associate II
Posted on May 17, 2011 at 14:11

Hello VLINE,

Is such patch file is available for STM32L1XX versions?

Thanks.

kenn
Associate II
Posted on May 17, 2011 at 14:11

I have a similar problem, Using Embedded Workbench 6.0 Evaluation Edition:

Thu Feb 10 12:12:33 2011: C:\Program Files\IAR Systems\Embedded Workbench 6.0 Evaluation\arm\config\flashloader\ST\FlashSTM32F10xxx.mac(5,20): Error: Operation error.  

Thu Feb 10 12:12:33 2011: Error while calling macro execUserFlashInit 

Thu Feb 10 12:12:33 2011: Failed to load flash loader: C:\Program Files\IAR Systems\Embedded Workbench 6.0 Evaluation\arm\config\flashloader\ST\FlashSTM32F100xB.flash 

This occurs when using the STM32Discovery SWD ports to flash an external STM32F103VB. I wonder if the wires are a problem, as I have a relatively long squid (>20cm). However STM's ST-Link Utility has absolutely no problem flashing the chip and verifying, so this would seem to indicate a problem with EW.

Any ideas?

Posted on May 17, 2011 at 14:11

C:\Program Files\IAR Systems\Embedded Workbench 6.0 Evaluation\arm\config\flashloader\ST\FlashSTM32F100xB.flash 

 

Any ideas?

Perhaps you have not selected the correct target device for the project? ie an F103, not the F100

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..