2009-06-11 8:55 AM
UM0424 for V2.0 lib
2011-05-17 4:14 AM
I could do with an older version of UM0424 which is targetted at the V2.0 libs.
My project is built with V2.0, and I need to add some USB functionality, so it would be easier to use the older UM0424 rather than port my project up to V3.0. Anybody know where I can get it from? Thanks, Chris.2011-05-17 4:14 AM
Panic over - I found a copy locally......
Chris.2011-05-17 4:14 AM
Hi,
Be aware that we keep an archive here :http://www.st.com/stonline/products/support/micro/files/stm32f10x_fw_archive.zip
and a patch is available to fix some limitations. Cheers, STOne-32.