cancel
Showing results for 
Search instead for 
Did you mean: 

Ultra Low Power Application without USB - what to do with VDDUSB?

gilberto-falker
Associate III

Hi

 

We are working on a project based on the STM32U073CCT6. The USB interfaces is not need. How should I connect the VDDUSB pin in order to minimize tthe power consuption? Is it Ok to connect it do GND?

 

Br

Gilberto

4 REPLIES 4
AScha.3
Super User

Hi,

read in ds...general/minimum working conditions.

->

AScha3_0-1758048396687.png

AScha3_1-1758048479654.png

 

If you feel a post has answered your question, please click "Accept as Solution".
FBL
ST Employee

Hi @gilberto-falker 

Check this article FAQ: Configuring the VDD50USB and VDD33USB pins on... - STMicroelectronics Community

It should be helpful.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL
Andrew Neil
Super User

@gilberto-falker wrote:

The USB interfaces is not need


The STM32U0 series Product Selector lists 12 models with no USB.

Could you use one of them?

A complex system that works is invariably found to have evolved from a simple system that worked.
A complex system designed from scratch never works and cannot be patched up to make it work.
gilberto-falker
Associate III

Hi

Models without usb have less flash memory