Skip to main content
martin_stojanovski93
Associate II
September 16, 2013
Question

UDIS/ URS - Bit, stm32F3

  • September 16, 2013
  • 1 reply
  • 1217 views
Posted on September 16, 2013 at 20:54

Hello my dear Forumers,

I'm having difficulties to understand the Update Disable bit and Update Request bit.

In the peripherial libs it is said, and i quote:

Configures the TIMx Update Request Interrupt source.

  * @param  TIMx: where x can be 1, 2, 3, 4, 6 ,7 ,8, 15, 16 or 17 to select the TIM peripheral.

  * @param  TIM_UpdateSource: specifies the Update source.

  *          This parameter can be one of the following values:

  *            @arg TIM_UpdateSource_Regular: Source of update is the counter

  *                 overflow/underflow or the setting of UG bit, or an update

  *                 generation through the slave mode controller.

  *            @arg TIM_UpdateSource_Global: Source of update is counter overflow/underflow.

  * @retval None

  */

void TIM_UpdateRequestConfig(TIM_TypeDef* TIMx, uint16_t TIM_UpdateSource)

and if i set the UDIS bit it says that the Update Event is NOT generated by the timer itself ( counting overflow) but if i MANUALLY set the UG bit i will generate an interrupt?

Does this mean that whenever i set the UDIS bit

TIM_UpdateDisableConfig(TIM1,ENABLE);

and set the UG-BIT with  :

TIM1->EGR |= 1UL;

 an interrupt will be generated and the void TIM1_UP_TIM16_IRQHandler() will be called?

- Because the IRQ handler isnt executed when  active the UDIS-bit.

So to sum up. URS-setting : Only the timer itself( over/underflow ) can generate an interrupt

                      UDIS - setting : Only setting the UG-Bit can make an interrupt.

Thanks in advance, Martin
    This topic has been closed for replies.

    1 reply

    martin_stojanovski93
    Associate II
    September 16, 2013
    Posted on September 16, 2013 at 22:12

    I have run a few tests in the debugger and concluded that:

    Interrupts are activated ( the void TIM1_UP_TIM16_IRQHandler() {} is called ) :

    UR =

    RESET

     UDIS =

    RESET

     

    - Overload,Underload of Timer                                                            

    YES

    -Update Generate bit set in EGR register. (TIM1->EGR |= 1UL;)        

    YES

    UR =

    SET

     UDIS =

    RESET

     

    - Overload,Underload of Timer                                                            

    YES

    -Update Generate bit set in EGR register. (TIM1->EGR |= 1UL;)        

    NO

    UR =

    RESET

     UDIS =

    SET

     

    - Overload,Underload of Timer                                                            

    NO

    -Update Generate bit set in EGR register. (TIM1->EGR |= 1UL;)        

    NO

    PS: Be carefull, in the void TIM_UpdateRequestConfig() function the parameters were switch in my library. 

    By switcht i mean that the values of TIM_UpdateSource_Global and TIM_UpdateSource_Regular were mixed with eachother.

    Martin