cancel
Showing results for 
Search instead for 
Did you mean: 

UART_DMA Delay ?

nandyeezforu
Associate II
Posted on October 26, 2015 at 20:20

Hi,

I  have connected two MCU's through UART.

I want to send a string from MCU 1 to MCU 2.

once the MCU 1 sent the string it need to wait for some time to receive the reply from MCU 2.

If MCU 1 did not get any reply from MCU 2,it need to send back a string 'u there?'

How we can do this ?

I have tried the following with no success :(

I am really vey new for programming forgive me if you find error,

uint8_t txBuffer[10] = ''HELLO\r\n''

uint8_t txBufferN[15] = ''u there ? \r\n''

uint8_t  rxBuffer[20] ;

HAL_UART_Transmit_DMA

(&UartHandle, (

uint8_t

*)txBuffer, 10);

HAL_Delay(100);

HAL_UART_Receive_DMA

(&UartHandle, (

uint8_t

*)rxBuffer, 20);

HAL_Delay(1000);

if

(rxBuffer[0]==

'H'

&&rxBuffer[1]==

'A'

&&rxBuffer[2]==

'I'

)

      {

          txBuffer[0]=

'C'

;

          txBuffer[1]=

'I'

;

          txBuffer[2]=

'A'

;

          txBuffer[3]=

'O'

;

          txBuffer[4]=

'\r'

;

         txBuffer[5]=

'\n'

;

       

        HAL_UART_Transmit_DMA(&UartHandle, (

uint8_t

*)txBuffer, 10);

}

else

{

HAL_UART_Transmit_DMA

(&UartHandle, (

uint8_t

*)txBufferN, 15);

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0