2015-10-11 6:24 AM
Hello,
I tried to test the I2C interface on a STM32:
#include <stdio.h>
#include <stdlib.h>
#include ''diag/Trace.h''
#include ''stm32f4xx_hal.h''
#include ''stdint.h''
int
main(
int
argc,
char
* argv[])
{
GPIO_InitTypeDef init;
I2C_HandleTypeDef i2c1Handle;
uint8_t data[5] = {1,2,3,4,5};
/* CLKs enable only if needed */
__HAL_RCC_GPIOB_CLK_ENABLE();
__HAL_RCC_I2C1_CLK_ENABLE();
// SDL Port B8
init.Pin = GPIO_PIN_8;
init.Mode = GPIO_MODE_AF_OD;
init.Alternate = GPIO_AF4_I2C1;
init.Pull = GPIO_NOPULL;
HAL_GPIO_Init(GPIOB, &init);
init.Pin = GPIO_PIN_9;
HAL_GPIO_Init(GPIOB, &init);
i2c1Handle.Instance = I2C1;
i2c1Handle.Init.ClockSpeed = 100000;
// 100kHz
i2c1Handle.Init.AddressingMode = I2C_ADDRESSINGMODE_7BIT;
i2c1Handle.Init.DualAddressMode = I2C_DUALADDRESS_DISABLED;
i2c1Handle.Init.GeneralCallMode = I2C_GENERALCALL_DISABLED;
i2c1Handle.Init.NoStretchMode = I2C_NOSTRETCH_DISABLED;
i2c1Handle.Init.OwnAddress1 = 0x56;
HAL_I2C_Init(&i2c1Handle);
//HAL_I2C_Master_Transmit(&i2c1Handle, 0x3C, data, 1, 10000);
// Infinite loop
while
(1)
{
// Add your code here.
int
i = 0;
}
} I found out, that when I init the speed variable, the program works. But now my question:
Does the variables don't have an init value, because the registers have init values?
2015-10-11 6:59 AM
Timing register is initialized to 0x0 upon reset. That's why you have to setup proper clock speed parameters based on your CPU clock in order for i2c to work properly.
2015-10-13 10:23 AM
Yes, but the gpio speed register was initialized with low speed.
But in the hal_gpio_init(...) is a assert_param(IS_GPIO_SPEED(GPIO_Init->Speed)); this assert crashes every time until I added the speed parameter. But why these variables don't have init values?2015-10-15 9:15 AM
Hi marmsoler.martinn,
This seems to be your own code, not a CubeMX generated one...-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2015-10-26 1:30 PM
I programm under linux with eclipse.