2016-06-11 11:51 PM
Hi!
Im trying to use two EXTI on PE2 and PE3 pins simultaneously. Two push bottons are connected to these two pins with a pull-up resistor and a capacitor filter prohibitting debounce phenomenon. As shown in the code below, in one ISR ''h'' is increased and in the other ''n''. the problem is that when I press one of the bottoms both ''h'' and ''n'' increase multiple times. On oscope PE2 and PE3 signals are correct but the stm32f4 processor is unpredictable. I don't understand what is happening!#include ''stm32f4xx.h''EXTI_InitTypeDef EXTI_InitStructure;GPIO_InitTypeDef GPIO_InitStructure;NVIC_InitTypeDef NVIC_InitStructure;uint16_t n,h=0;static void EXTI_Configuration(void);int main(void){ SystemInit(); // SysTick_Config(SystemCoreClock/1000); EXTI_Configuration(); while(1);}static void EXTI_Configuration(void){ RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOE , ENABLE); RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE); GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN; GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructure.GPIO_Pin =GPIO_Pin_2|GPIO_Pin_3; GPIO_Init(GPIOE, &GPIO_InitStructure); SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOE, EXTI_PinSource2); SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOE, EXTI_PinSource3); EXTI_InitStructure.EXTI_Line = EXTI_Line2|EXTI_Line3; EXTI_InitStructure.EXTI_LineCmd = ENABLE; EXTI_InitStructure.EXTI_Mode = EXTI_Mode_Interrupt; EXTI_InitStructure.EXTI_Trigger = EXTI_Trigger_Falling; EXTI_Init(&EXTI_InitStructure); NVIC_InitStructure.NVIC_IRQChannel = EXTI2_IRQn; NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0; NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1; NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE; NVIC_Init(&NVIC_InitStructure); NVIC_InitStructure.NVIC_IRQChannel = EXTI3_IRQn; NVIC_Init(&NVIC_InitStructure);}void EXTI2_IRQHandler(void){ if(EXTI_GetITStatus(EXTI_Line2) != RESET) { n++; EXTI_ClearITPendingBit(EXTI_Line2); //Clear the EXTI line 2 pending bit }}void EXTI3_IRQHandler(void){ if(EXTI_GetITStatus(EXTI_Line3) != RESET) { h++; EXTI_ClearITPendingBit(EXTI_Line3); }}2016-06-12 12:27 AM
Hm, I would not expect a simple capacitor to be sufficient to prevent bounces on a pushbutton.
But if you meant that a single press on button 1 increments _both_ ''h'' and ''n'', then I would double-check the hardware for shorts. BTW, you should declare the ''h'' and ''n'' counters as volatile when they are updated in an interrupt. Hope this helps, - Kristian.2016-06-12 4:07 AM
Thanks for your reply Kristian!
I think parameter definition is not the point, since when i tried to set and reset PC10 in one ISR and PC11 in the other, this conflict happened again.By the way what would you recommend to prevent bounce on a pushbotton?2016-06-12 8:49 AM
buttons + external interrupts = stupidity,
Check buttons in timer interrupt in period 50-100ms.